How to use any LPCexpresso board to program other LPC controllers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use any LPCexpresso board to program other LPC controllers

2,918 Views
naveenkumar_b
Contributor II

Hi,

I am using LPCexpresso802 board. I have made a product using LPC802 controller. Now I am looking for a programmer. So far I used LPCexpresso board to implement my application. Now I need to program my customized board. I am planning to use LPCexpresso board as a programmer I don't know how. Something like, We can use STM32 Debugger which is available in the Evaluation kit as a programmer to program any external STM32 controllers.

I don't see any information in User manual. It will be great if some one could tell me what programmer is best. I remember earlier with LPC1114 I used built in Debugger to program other controllers too.

Thanks,

Naveen

Labels (2)
3 Replies

2,760 Views
naveenkumar_b
Contributor II

Thanks Guys,

I have ordered LPC Link.

Regards,

Naveen

0 Kudos
Reply

2,760 Views
converse
Senior Contributor V

Why not just buy an lpc-link2? They are designed to run standalone and can be bought from Amazon for less than $25, saving a lot of hassle.

2,760 Views
BlackNight
NXP Employee
NXP Employee

You find that information usually in the documentation for the board or have a look at the schematics. See as well Using the LPCXpresso V2/V3 Boards to Debug an external Board | MCU on Eclipse 

I hope this helps,

Erich