Where is demo application for LPCXpresso1125?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is demo application for LPCXpresso1125?

1,008 Views
edconrad
Contributor I

Where is demo application for LPCXpresso1125?

lpcopen_2_17_lpcxpresso_1125.zip does not contain the application shipped with the board.

Thanks,

EC

0 Kudos
Reply
1 Reply

956 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ed,

    lpcopen_2_17_lpcxpresso_nxp_lpcxpresso_1125 just have the peripherals project and the freertos_blinky project.

   These project provide the code for the detail peripherals.

    For the detail demo application, normally, customer need to write it by themselves.


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply