What tools can I use to download images after securely booting of LPC54S018?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What tools can I use to download images after securely booting of LPC54S018?

跳至解决方案
1,689 次查看
827529957
Contributor III

The LPC54S018 disables SWD once Secure Boot is turned on. In other words, after I start the secure boot, if I want to download the new correctly encrypted image, do I have to enter the ISP mode to download?
I only know that the flash magic tool can be used to download images in ISP mode. I read the signature successfully, but failed to use it to download a plain image. The error it returns is as follows. Snap10.bmpAre there other recommended tools that can be downloaded in ISP mode?

标签 (1)
0 项奖励
回复
1 解答
1,479 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kunsen,

When secure boot is completed successfully, the SWD will followed the OTP fields (SWD_EN0 and SWD EN1). Below flow chart in UM is correct.

pastedImage_1.png

I suggest that you uses a flash programmer to program a correct secure image into external flash.

And please be careful when config OTP, there is an application note, you can have a look:

https://www.nxp.com/docs/en/nxp/application-notes/AN12352.pdf    

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,479 次查看
827529957
Contributor III

The most important question is that, after LPC54S018 securely booting with SWD disabled, what tools I can use to download a new correctly encrypted image?  I hope you can recommend a viable tool for me. Thank you.

0 项奖励
回复
1,480 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kunsen,

When secure boot is completed successfully, the SWD will followed the OTP fields (SWD_EN0 and SWD EN1). Below flow chart in UM is correct.

pastedImage_1.png

I suggest that you uses a flash programmer to program a correct secure image into external flash.

And please be careful when config OTP, there is an application note, you can have a look:

https://www.nxp.com/docs/en/nxp/application-notes/AN12352.pdf    

0 项奖励
回复