What should the LPC84x FLASHTIM register be set to?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What should the LPC84x FLASHTIM register be set to?

跳至解决方案
1,362 次查看
george
Senior Contributor II

Hello Team,

My customers are using LPC845 and they frequently encounter a HardFault while debugging.

Their painstaking analysis revealed that it was related to the FLASHTIM register.
They are using a 30MHz system clock, in which case setting FLASHTIM=1 will prevent the HardFault.

I found similar posts in the community, but the Flash access time specifications are not clear here.
https://community.nxp.com/t5/LPC-Microcontrollers/LPC8xx-Flash-access-time-aka-setting-FLASHTIM/m-p/...

In other LPC series it is clearly stated in UM.
Ex LPC111x :
george_3-1730045412297.png

Ex LPC546xx :
george_4-1730045752630.png

However, this point is not clearly stated in the LPC84x UM.

george_5-1730045840042.png

Please clarify the specifications related to FLASHTIM so that customers can freely handle the system clock.

Thanks,
George

 

 

 

 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,327 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose the SDK team has addressed the issue.

Pls download SDK package from the website:

https://mcuxpresso.nxp.com/en

The SDK version has updated to 2.16.000, which has added a function void CLOCK_SetFLASHAccessCyclesForFreq(uint32_t iFreq) to solve the issue.

xiangjun_rong_0-1730172367562.png

 

/*! brief Set the flash wait states for the input freuqency.
* param iFreq : Input frequency
*/
void CLOCK_SetFLASHAccessCyclesForFreq(uint32_t iFreq)
{
uint32_t num_wait_states;
if (iFreq <= 24000000UL)
{
/* [0 - 24 MHz] */
num_wait_states = 0UL;
}
else
{
/* Above 24 MHz */
num_wait_states = 1UL;
}

FLASH_CTRL->FLASHCFG =
((FLASH_CTRL->FLASHCFG & ~FLASH_CTRL_FLASHCFG_FLASHTIM_MASK) | FLASH_CTRL_FLASHCFG_FLASHTIM(num_wait_states));
}

 

when the core frequency is less than 24MHz, 1 clock cycle is added. when the core frequency is above 24MHz, 2 clock cycle is added. 

For the user manual update, it requires time.

Hope it can help you

BR

XiangJun Rong

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,328 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose the SDK team has addressed the issue.

Pls download SDK package from the website:

https://mcuxpresso.nxp.com/en

The SDK version has updated to 2.16.000, which has added a function void CLOCK_SetFLASHAccessCyclesForFreq(uint32_t iFreq) to solve the issue.

xiangjun_rong_0-1730172367562.png

 

/*! brief Set the flash wait states for the input freuqency.
* param iFreq : Input frequency
*/
void CLOCK_SetFLASHAccessCyclesForFreq(uint32_t iFreq)
{
uint32_t num_wait_states;
if (iFreq <= 24000000UL)
{
/* [0 - 24 MHz] */
num_wait_states = 0UL;
}
else
{
/* Above 24 MHz */
num_wait_states = 1UL;
}

FLASH_CTRL->FLASHCFG =
((FLASH_CTRL->FLASHCFG & ~FLASH_CTRL_FLASHCFG_FLASHTIM_MASK) | FLASH_CTRL_FLASHCFG_FLASHTIM(num_wait_states));
}

 

when the core frequency is less than 24MHz, 1 clock cycle is added. when the core frequency is above 24MHz, 2 clock cycle is added. 

For the user manual update, it requires time.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复
1,319 次查看
george
Senior Contributor II

Hello @xiangjun_rong 

Thanks for the reply, as far as I know I can't find that information anywhere in the NXP documentation.

In other words, So does that mean the flash access time needs to be 24MHz or less as a chip specification?

Thanks,
George

0 项奖励
回复
1,310 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, the section  6.4.1 Flash configuration register in UM11029.pdf has not any update till now.

But the SDK package adds a function to set up the FLASHTIM bits in FLASHCFG reg.

The core frequency of LPC84x can reach up to 30MHz, if the core frequency is less than 24Mhz, you set the FLASHTIM bits as 0, which means 1 clock cycle delay. if the core frequency is equal or greater than 24Mhz and less than 30Mhz, you set the FLASHTIM bits as 1, which means 2 clock cycle delay.


The void CLOCK_SetFLASHAccessCyclesForFreq(uint32_t iFreq) api function input variable is the actual core frequency, it set up the FLASHTIM bits based on the core frequency.

 

xiangjun_rong_0-1730195583028.png

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复
1,297 次查看
george
Senior Contributor II

hello @xiangjun_rong,

There is no sample code that uses the CLOCK_SetFLASHAccessCyclesForFreq() in the latest SDK, so few users will notice its existence.

In any case, our question is answered.
Thank you for your detailed answer.

BR,
George 

0 项奖励
回复