What precautions must be taken to avoid overwrite of program space in FLASH memory?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What precautions must be taken to avoid overwrite of program space in FLASH memory?

跳至解决方案
1,646 次查看
athmesh_n
Contributor IV

Will writing inside FLASH memory overwrite the program inside the FLASH memory? If so what are the precautions that need to be taken to avoid problems?

Processor   :   LPC 1517

IDE             :   LPCXpresso v8.2.2 [Build 650] [2016-09-09]

标签 (1)
1 解答
1,509 次查看
soledad
NXP Employee
NXP Employee

Hi,

There are three key issues with using flash memory:

• Erasing memory is on a per-sector basis

• Flash memory lifespan

• Reprogramming locations

Please check the attached application note.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,510 次查看
soledad
NXP Employee
NXP Employee

Hi,

There are three key issues with using flash memory:

• Erasing memory is on a per-sector basis

• Flash memory lifespan

• Reprogramming locations

Please check the attached application note.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------