What is the maximum current value from GPIO/PWM pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the maximum current value from GPIO/PWM pin?

3,407 Views
jacob_
Contributor I

Hi everyone,

I am going to use GPIO pin as output/PWM output to drive N-MOSFET gate with logic level voltage input (e.g. International Rectifier IRLR2905Z or IRLR3705Z). I need to know what is the maximum current value of this pin to calculate the proper value of input gate resistor limited first current pulse while turning on the N-MOSFET thru gate capacity. I tried to found it in the UM10360 datasheet but with no result.

Best regards,

Jacob

Labels (2)
0 Kudos
Reply
1 Reply

2,895 Views
soledad
NXP Employee
NXP Employee

Hello Jacob,

Please check the following datasheet of the LPC1769  

https://cache.nxp.com/docs/en/data-sheet/LPC1769_68_67_66_65_64_63.pdf 

In table 8. Static Characteristics you are going to found the value required.  

Best Regards ,

TIC

0 Kudos
Reply