What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ?

3,329 次查看
atkinsd84
Contributor I

Hi everyone, I'm struggling with how to terminate unused pins and the data sheet doesn't appear to have all the answers.  Can anyone help me with how to terminate pins 16 and 18 on the LPC1768 when not using the RTC.

标签 (1)
0 项奖励
回复
2 回复数

3,103 次查看
soledad
NXP Employee
NXP Employee

Hi David,

I would recommend that RTCX1 be grounded since it is an input. RTCX2 is an output, so it can be left open.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,100 次查看
atkinsd84
Contributor I

Thanks

David Atkins

Land & Naval Defence Electronics Division

Leonardo MW Ltd

20A1-2 Ground Floor Southside PO Box 5

Southmead Road

Filton

Bristol

BS34 7QW

david.atkins@leonardocompany.com<mailto:david.atkins@leonardocompany.com>

Tel: +44 (0) 117 931 3556

Mob: +44 (0) 7793422675

HELICOPTERS / AERONAUTICS / ELECTRONICS, DEFENCE AND SECURITY SYSTEMS / SPACE

0 项奖励
回复