What could be practical reason for using two 1MB Static RAM chips on LPC1788?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What could be practical reason for using two 1MB Static RAM chips on LPC1788?

Jump to solution
2,511 Views
Eugene723
Contributor II

I recently took on support for a board designed by others about 10 years ago. There are two 8Mbit (1MB) CY7C1051 chips on this board.

LPC1788 has four Chip Selects (CS0 through CS3) each supporting up to 64MB of static RAM.

I don’t have much hardware design knowledge hence my question. I briefly checked on pricing and noticed that one 4MB chip costs about as much as two 1MB while providing two times memory amount.

What could be the reason to design two separate 1MB chips as opposite to one of a larger size?

 

Thank you,

 

Eugene

Labels (1)
0 Kudos
Reply
1 Solution
2,436 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

"I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4."

->> For LPC1788, no such limitation.

"one 4MB chip costs about as much as two 1MB while providing two times memory amount."

->> Recommend using one 4MB chip as this situation.

 

BR

Alice

View solution in original post

0 Kudos
Reply
3 Replies
2,461 Views
Eugene723
Contributor II

Thank you, Alice.

 

These chips are used for background and foreground frames for LCD so, if one were broken the entire board would stop functioning…

 

I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4.

 

Eugene

0 Kudos
Reply
2,437 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

"I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4."

->> For LPC1788, no such limitation.

"one 4MB chip costs about as much as two 1MB while providing two times memory amount."

->> Recommend using one 4MB chip as this situation.

 

BR

Alice

0 Kudos
Reply
2,468 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

 

Maybe one SRAM is broken, anther one can used. 

Also for the chip costs, you need check the same company and same series.

 

BR

Alice