What could be practical reason for using two 1MB Static RAM chips on LPC1788?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What could be practical reason for using two 1MB Static RAM chips on LPC1788?

跳至解决方案
2,593 次查看
Eugene723
Contributor II

I recently took on support for a board designed by others about 10 years ago. There are two 8Mbit (1MB) CY7C1051 chips on this board.

LPC1788 has four Chip Selects (CS0 through CS3) each supporting up to 64MB of static RAM.

I don’t have much hardware design knowledge hence my question. I briefly checked on pricing and noticed that one 4MB chip costs about as much as two 1MB while providing two times memory amount.

What could be the reason to design two separate 1MB chips as opposite to one of a larger size?

 

Thank you,

 

Eugene

标签 (1)
0 项奖励
回复
1 解答
2,518 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

"I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4."

->> For LPC1788, no such limitation.

"one 4MB chip costs about as much as two 1MB while providing two times memory amount."

->> Recommend using one 4MB chip as this situation.

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,543 次查看
Eugene723
Contributor II

Thank you, Alice.

 

These chips are used for background and foreground frames for LCD so, if one were broken the entire board would stop functioning…

 

I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4.

 

Eugene

0 项奖励
回复
2,519 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

"I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4."

->> For LPC1788, no such limitation.

"one 4MB chip costs about as much as two 1MB while providing two times memory amount."

->> Recommend using one 4MB chip as this situation.

 

BR

Alice

0 项奖励
回复
2,550 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

 

Maybe one SRAM is broken, anther one can used. 

Also for the chip costs, you need check the same company and same series.

 

BR

Alice