What could be practical reason for using two 1MB Static RAM chips on LPC1788?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What could be practical reason for using two 1MB Static RAM chips on LPC1788?

ソリューションへジャンプ
2,480件の閲覧回数
Eugene723
Contributor II

I recently took on support for a board designed by others about 10 years ago. There are two 8Mbit (1MB) CY7C1051 chips on this board.

LPC1788 has four Chip Selects (CS0 through CS3) each supporting up to 64MB of static RAM.

I don’t have much hardware design knowledge hence my question. I briefly checked on pricing and noticed that one 4MB chip costs about as much as two 1MB while providing two times memory amount.

What could be the reason to design two separate 1MB chips as opposite to one of a larger size?

 

Thank you,

 

Eugene

ラベル(1)
0 件の賞賛
返信
1 解決策
2,405件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

"I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4."

->> For LPC1788, no such limitation.

"one 4MB chip costs about as much as two 1MB while providing two times memory amount."

->> Recommend using one 4MB chip as this situation.

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,430件の閲覧回数
Eugene723
Contributor II

Thank you, Alice.

 

These chips are used for background and foreground frames for LCD so, if one were broken the entire board would stop functioning…

 

I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4.

 

Eugene

0 件の賞賛
返信
2,406件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

"I just wanted to verify that there is no some sort of “symmetrical” reason - as for example, in desktop PCs it’s required to plug identical memory modules in slots 1 and 3; then 2 and 4."

->> For LPC1788, no such limitation.

"one 4MB chip costs about as much as two 1MB while providing two times memory amount."

->> Recommend using one 4MB chip as this situation.

 

BR

Alice

0 件の賞賛
返信
2,437件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eugene723 

 

Maybe one SRAM is broken, anther one can used. 

Also for the chip costs, you need check the same company and same series.

 

BR

Alice