What are the difference between LPC4330FET180,551, LPC4330FET180/3D and LPC4330FET180Y ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the difference between LPC4330FET180,551, LPC4330FET180/3D and LPC4330FET180Y ?

1,368 Views
MadhuriAkkenepa
Contributor II

What are the difference between part numbers LPC4330FET180,551, LPC4330FET180/3D and LPC4330FET180Y ?

0 Kudos
Reply
1 Reply

1,282 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

They are the unique, complete order number for the devices and the order number also includes the packing information.

2016-09-01_11-08-17.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply