What are the difference between LPC4330FET180,551, LPC4330FET180/3D and LPC4330FET180Y ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the difference between LPC4330FET180,551, LPC4330FET180/3D and LPC4330FET180Y ?

1,369件の閲覧回数
MadhuriAkkenepa
Contributor II

What are the difference between part numbers LPC4330FET180,551, LPC4330FET180/3D and LPC4330FET180Y ?

0 件の賞賛
返信
1 返信

1,283件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

They are the unique, complete order number for the devices and the order number also includes the packing information.

2016-09-01_11-08-17.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信