Want to add UART communication in NFCrdlibEx4_Mifareclassic code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Want to add UART communication in NFCrdlibEx4_Mifareclassic code

1,193件の閲覧回数
suhas_badve1
Contributor I

Hi All,

I am using CLEV6630B board for RFID reader and want to read/write on Mifare classic card.

I am using NFCrdlibEx4_Mifareclassic library code. I want to add UART communication in this code so that I can connect the board to PC over serial and send the card information to PC. 

I want to develop PC based software through which I can send the commands to the CLEV6630B board to write some data in the Mifare Classic card, read data from Mifare Classic card etc. In short I want to add UART interface on TXD0 and RXD0 (which is available on CLEV6630B) in NFCrdlibEx4_Mifareclassic code

Please guide. Please share some sample code.

Thanks.

0 件の賞賛
返信
1 返信

1,146件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @suhas_badve1

We will continue the communication in your internal ticket.

Have a nice day!

Regards,
Eduardo.

0 件の賞賛
返信