Want to add UART communication in NFCrdlibEx4_Mifareclassic code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Want to add UART communication in NFCrdlibEx4_Mifareclassic code

1,180 Views
suhas_badve1
Contributor I

Hi All,

I am using CLEV6630B board for RFID reader and want to read/write on Mifare classic card.

I am using NFCrdlibEx4_Mifareclassic library code. I want to add UART communication in this code so that I can connect the board to PC over serial and send the card information to PC. 

I want to develop PC based software through which I can send the commands to the CLEV6630B board to write some data in the Mifare Classic card, read data from Mifare Classic card etc. In short I want to add UART interface on TXD0 and RXD0 (which is available on CLEV6630B) in NFCrdlibEx4_Mifareclassic code

Please guide. Please share some sample code.

Thanks.

0 Kudos
Reply
1 Reply

1,133 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @suhas_badve1

We will continue the communication in your internal ticket.

Have a nice day!

Regards,
Eduardo.

0 Kudos
Reply