Wakeup signal while in active mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wakeup signal while in active mode

1,397 Views
dimitrissideris
Contributor III

Hi there,

I was checking the datasheet but i couldnt find this.

If lpc43xx is in active mode and a wakeup signal occurs what will happen?

Is the signal discarted or device reboots?

Labels (1)
0 Kudos
Reply
1 Reply

1,255 Views
soledad
NXP Employee
NXP Employee

Hi,

It is neither of both, the Interrupt of the Signal gets into the device, but since the device it is in Active Mode, remains in the same estate.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply