Wakeup signal while in active mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wakeup signal while in active mode

1,391 次查看
dimitrissideris
Contributor III

Hi there,

I was checking the datasheet but i couldnt find this.

If lpc43xx is in active mode and a wakeup signal occurs what will happen?

Is the signal discarted or device reboots?

标签 (1)
0 项奖励
回复
1 回复

1,249 次查看
soledad
NXP Employee
NXP Employee

Hi,

It is neither of both, the Interrupt of the Signal gets into the device, but since the device it is in Active Mode, remains in the same estate.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复