Vrefn maximum

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vrefn maximum

2,666 Views
vaque
Contributor II

Hi all;

I need to know the minimum value of Vrefn. I suppose that according with the manual ((Vrefp-Vrefn)/2) + Vrefn = Vdd/2. Therefore Vrefnmaximum = Vdd - Vrefminimum.

If Vdd=3.3v and Vrefminimum is 2.4v (acording with the manual).

Is Vrefnmaximum 0.9v and then is the maximum sensibility 0.366 mV?

Thanks so much and regards. Daniel.

Labels (2)
0 Kudos
Reply
4 Replies

2,489 Views
vaque
Contributor II

Yes, I am using a LPC824.

Regards. Daniel.

0 Kudos
Reply

2,489 Views
soledad
NXP Employee
NXP Employee

Hi,

Yes, Vrefn max= 0.9v however

1 LSB = (Vrefp - Vss)/4096 according with the datasheet

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,489 Views
vaque
Contributor II

Hi Soledad;

LPC82x.pdf Fig 39 image does not indicates a conection between Vrefn and Vss?

I don't understand... Vrefn does not fix the minimum value of the full scale (FS)?

I thought that result of a conversion is:

form3.png

*A parenthesis between (Vinn-Vrefn) is mising)

But in UM10800.pdf at page 322 "Perform a single ADC conversion using a software trigger"  it says that The result of the conversion is (4095 x VIN)/(VREFP - VREFN).

On one hand this would mean that there isn't an Vrefn offset and on the other hand this would mean that LSB (minimum)[v] ocurrs when Vrefp(minimum) and Vrefn(maximum):

form4.png

I need more information about the problem please.

Regards. Daniel.

0 Kudos
Reply

2,489 Views
soledad
NXP Employee
NXP Employee

Hello Daniel,

Could you please mention the device you are using?

Regards

Sol

0 Kudos
Reply