Vdd on HVQFN33 package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vdd on HVQFN33 package

1,065件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cyberstudio on Sat May 03 12:20:48 MST 2014
The User Manual says pin 6 and pin 29 are Vdd connections, powering the ADC, IO pins, the processor, etc. They are not internally connected together and both must be powered.

My question is, is it pin 6 or pin 29 powering the USB PLL for the LPC11Uxx part?

(I am just trying to learn whether pin 6 or pin 29 will more likely have more RF noise, if you are wondering why I am asking this question. That's all.)
ラベル(1)
0 件の賞賛
返信
1 返信

1,042件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Fri May 16 16:37:51 MST 2014
Hi,

Pin 29 will be powered the USB PLL.

Thanks.

nxp_support
0 件の賞賛
返信