Vdd on HVQFN33 package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vdd on HVQFN33 package

1,061 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cyberstudio on Sat May 03 12:20:48 MST 2014
The User Manual says pin 6 and pin 29 are Vdd connections, powering the ADC, IO pins, the processor, etc. They are not internally connected together and both must be powered.

My question is, is it pin 6 or pin 29 powering the USB PLL for the LPC11Uxx part?

(I am just trying to learn whether pin 6 or pin 29 will more likely have more RF noise, if you are wondering why I am asking this question. That's all.)
Labels (1)
0 Kudos
Reply
1 Reply

1,038 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Fri May 16 16:37:51 MST 2014
Hi,

Pin 29 will be powered the USB PLL.

Thanks.

nxp_support
0 Kudos
Reply