Variation in current consumption for different offsets in memory regions why?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Variation in current consumption for different offsets in memory regions why?

1,530件の閲覧回数
himanshudoshi
Contributor III

Hello to all,

I am trying to figure out the variation in current consumption as well as in clock cycles due to different memory regions and different offsets. During various experiments, I have found the following results:

LDR R4,[R1,#0x0]  (R1 = 0x00000000 (Flash) with 0 offset)  :   Current = 2.60mAmps & Cycles = 2

LDR R4,[R1,#0x1]  (R1 = 0x00000000 (Flash) with 1 offset)  :   Current = 2.07mAmps & Cycles = 4

LDR R4,[R1,#0x2]  (R1 = 0x00000000 (Flash) with 2 offset)  :   Current = 2.30mAmps & Cycles = 3

LDR R4,[R1,#0x3]  (R1 = 0x00000000 (Flash) with 3 offset)  :   Current = 2.08mAmps & Cycles = 4

from offset 4 it repeats the order. I mean Offset = 4 is equal to Offset = 0 ; Offset = 5 is equal to Offset = 1Offset = 6 is equal to Offset = 2Offset = 7 is equal to Offset = 3Offset = 8 is equal to Offset = 0  and so on.... 

Similarly, while access SRAMX also :

 

LDR R4,[R1,#0x0]  (R1 = 0x04000000 (Flash) with 0 offset)  :   Current = 2.88mAmps & Cycles = 1

LDR R4,[R1,#0x1]  (R1 = 0x04000000 (Flash) with 1 offset)  :   Current = 2.30mAmps & Cycles = 3

LDR R4,[R1,#0x2]  (R1 = 0x04000000 (Flash) with 2 offset)  :   Current = 2.65mAmps & Cycles = 2

LDR R4,[R1,#0x3]  (R1 = 0x04000000 (Flash) with 3 offset)  :   Current = 2.29mAmps & Cycles = 3

from offset 4 it repeats the order. I mean Offset = 4 is equal to Offset = 0 ; Offset = 5 is equal to Offset = 1 Offset = 6 is equal to Offset = 2 Offset = 7 is equal to Offset = 3 Offset = 8 is equal to Offset = 0  and so on.... 

On the basis of observation, I have two question:

  1. Why different offset value, results into different current consumption?
  2. What is the reason for current variations, while accessing different memory regions?

Kindly help me out with this. I am using LPCXpresso 54114  board, with ARM Cortex-M4 processor. And all the measurement have been taken at 12MHz.

Thanking you,

Regards,

Himanshu

ラベル(4)
0 件の賞賛
返信
1 返信

1,390件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi HIMANSHU DOSHI ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
I'd like to get the more information, for instance, whether you can introduce the testing steps in details.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信