VC++ project files for emwin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VC++ project files for emwin

1,324件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravi Teja on Thu May 17 03:15:12 MST 2012
Hi

  For emwin graphics library they mentioned about VC++ project files but they didn't given any VC++ project files in both the libraries and BSP . IS it a paid service or we can get for free? In the BSP which we have downloaded the following path NXP\emWin\Start\Sample\Tutorial contains so many example problems are we have to run these problems using VC++ for that no project files they have given.Where we can get these

Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,243件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Thu May 17 06:32:55 MST 2012
They should be in the base directory of the BSPs. They are called simulation.sln and simulation.vcxproj.
0 件の賞賛
返信