VC++ project files for emwin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VC++ project files for emwin

1,333 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravi Teja on Thu May 17 03:15:12 MST 2012
Hi

  For emwin graphics library they mentioned about VC++ project files but they didn't given any VC++ project files in both the libraries and BSP . IS it a paid service or we can get for free? In the BSP which we have downloaded the following path NXP\emWin\Start\Sample\Tutorial contains so many example problems are we have to run these problems using VC++ for that no project files they have given.Where we can get these

Thanks
标签 (1)
0 项奖励
回复
1 回复

1,252 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Thu May 17 06:32:55 MST 2012
They should be in the base directory of the BSPs. They are called simulation.sln and simulation.vcxproj.
0 项奖励
回复