Using emWin with LPC1227 and small LCD Module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using emWin with LPC1227 and small LCD Module

982 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tdl on Fri Nov 29 20:41:25 MST 2013
I am using an LPC1227 with a small 128x128 color LCD, connected using SPI.  The LCD has a Philips PCF8833 controller.

Is it possible for me to use the LPC licensed emWin libraries with this?  This controller is not specifically mentioned in the emWin 5.22 reference, I have written code in the past to draw to this display directly, but I wanted to take advantage of the driver abstraction provided by emWin because the LCD may be changed out for one with a different controller in the future.  Given the datasheet for this controller, should I be able to configure an existing driver to work?

Any direction would be appreciated.

标签 (1)
0 项奖励
回复
0 回复数