Using emWin with LPC1227 and small LCD Module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using emWin with LPC1227 and small LCD Module

978件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tdl on Fri Nov 29 20:41:25 MST 2013
I am using an LPC1227 with a small 128x128 color LCD, connected using SPI.  The LCD has a Philips PCF8833 controller.

Is it possible for me to use the LPC licensed emWin libraries with this?  This controller is not specifically mentioned in the emWin 5.22 reference, I have written code in the past to draw to this display directly, but I wanted to take advantage of the driver abstraction provided by emWin because the LCD may be changed out for one with a different controller in the future.  Given the datasheet for this controller, should I be able to configure an existing driver to work?

Any direction would be appreciated.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)