Using I2S DMA with mono Audio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using I2S DMA with mono Audio

3,983 Views
jacintomoreno
Contributor III

Hi,

I am using the I2S with DMA, however I am using mono audio, I was wondering whether there is a way to use the DMA in mono, as I don't want to just copy the same data to the other channel as I don't need it.

Thank in advance for your help.

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

3,576 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jacinto,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

3,576 Views
jacintomoreno
Contributor III

Hi Carlos,

Have you had a chance to look at this?

0 Kudos
Reply

3,576 Views
jacintomoreno
Contributor III

Hi Carlos,

I am using LPC54605J512.

The problem I am facing is that I want to use I2S DMA in a mono mode, so I don't have to duplicate data because I am short of RAM memory.

I have configure the DMA and I2S as follows, using the Linked transfers (linked list) mode. However the last block of the buffer always produces a glitch, I am not sure what is going on...

/**
 * Channel transfer configuration.
**/
#define I2S_XFERCFG_INVALID (0 \
    | !DMA_XFERCFG_CFGVALID                     /* Not valid until s/w writes SETVALID reg */ \
    |  DMA_XFERCFG_RELOAD                       /* Follow next pointer to next descriptor */ \
    |  DMA_XFERCFG_SWTRIG                       /* Assert s/w triggering immediately */ \
    | !DMA_XFERCFG_CLRTRIG                      /* Don't clear trigger at end of txfer */ \
    |  DMA_XFERCFG_SETINTA                      /* Set interrupt A on end of txfer */ \
    | !DMA_XFERCFG_SETINTB                      /* Don't set interrupt B on end of txfer */ \
    |  DMA_XFERCFG_WIDTH_16                     /* I2S FIFO requires 32-bit accesses */ \
    |  DMA_XFERCFG_SRCINC_1                     /* Source (memory) increment of 1 access width */ \
    |  DMA_XFERCFG_DSTINC_0                     /* Destination (FIFO) does not increment */ \
    |  DMA_XFERCFG_XFERCOUNT(I2S_BLOCK_SIZE))   /* Transfer size is fixed at block size */

static const I2S_AUDIO_FORMAT_T sAudioFmtTx =
  {
    I2S_TX,     /*!< Data direction: tx or rx */
    NORMAL_MASTER,   /*!< Master / Slave configuration */
    I2S_CLASSIC,   /*!< I2S mode */
    false,     /*!< right channel data in low portion of FIFO */
    false,     /*!< left justify data in FIFO */
    false,     /*!< data source is the D-Mic subsystem */
    false,     /*!< SCK polarity */
    false,     /*!< WS polarity */
    2,      /*!< Flexcomm function clock divider; use MCLK/2 */
    1,      /*!< Channel Number - 1 is mono, 2 is stereo */
    16,      /*!< Word Width */
    32,      /*!< Frame Width */
    0,      /*!< Data position in the frame */
    0,      /*!< FIFO interrupt trigger depth: 0 trigger on empty */
  };

Jacinto

0 Kudos
Reply