如何把LPC1765的AHB RAM改成普通的RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

如何把LPC1765的AHB RAM改成普通的RAM

804 Views
yangw
Contributor I

查了下资料发现LPC1765的RAM有3部分组成,分别是平时使用的32K的RAM,AHB0的SRAM 16K,AHB1的SRAM 16K.那么我现在想把AHB0或AHB1的SRAM当成普通的RAM可以吗?网上查了下好像是要修改分散加载文件的,但是这个文件怎么改?

Labels (2)
0 Kudos
1 Reply

570 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 伟 杨,
非常感谢使用NXP产品,很高兴为你提供技术支持!
可以的,AHB RAM本身就是RAM,我不知道你说的改成普通的RAM的具体应用是什么,至于修改加载文件,我建议你可以在Keil的Help里搜索,那里是最官方的。
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos