Using CLEV663B Blueboard Rev3 with Raspberry Pi 3 and I2C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using CLEV663B Blueboard Rev3 with Raspberry Pi 3 and I2C

1,934 次查看
florianjouffrea
Contributor I

Hi everyone, 

For some time now, I'm trying to get the CLEV663B Blueboard Rev3 working with the Raspberry Pi. With no luck, I've tried using SPI and since I will have to use I2C in the end, I'm now trying to communicate via I2C. 

The CLEV663B is functionnal using a LPC11U68 and SPI. 

For my latest tests, you will find below my configuration : 

- NXPNFCRDLIB LINUX SW PACKAGE (v4.040.05.011646_20161115) , sw3693.zip.

   The only file modified in the package is the NxpNfcRdLib/types/ph_NxpBuild_Lpc.h and here the modifications :

 comment line 64 :

//#define NXPBUILD_PH_LPC1769

uncomment line 67 :

#define NXPBUILD_PH_RASPBERRY_PI

comment line 85 and uncomment line 86 :

//#define NXPBUILD_PHBAL_REG_LINUX_USER_SPI

#define NXPBUILD_PHBAL_REG_LINUX_USER_I2C

comment line 96 and uncomment line 97 : 

//#define NXPBUILD_PHHAL_HW_RC523

#define NXPBUILD_PHHAL_HW_RC663

Soldering on the CLEV663B :

I have removed R15, R26 and R21 and placed the 0R resistor on R29, R16 and R20 (as instructed in AN11211).

Pinout CLEV663B / RPi :

Following the file NxpNfcRdLib/intfs/phPlatform_Port_Pi_RC633.h, here how I connect my two devices : 

Pins for 3.3V, 5V and GND are classicaly connected. The USB alim is also connected.

Raspberry PI 3CLEV663B REV 3
PIN 3   (GPIO2)SDA
PIN 5   (GPIO3)SCL
PIN 7   (GPIO4)AD0
PIN 11 (GPIO17)AD1
PIN 13 (GPIO27)P2.4
PIN 15 (GPIO22)P2.5
PIN 16 (GPIO23)P3.3
PIN 18 (GPIO24)RST

First of all, when I use `i2cdetect` on Raspbian to find the slave adress of the blueboard, frames leave the RPi but no answer from the Blueboard. 

I deduce from the datasheet that the slave adress should be 0x28 (as configured in the config file). When I run the first example from the lib, I received the following error (continuously looping on it) :

Line : 189  Error - (0x010B) has occured : 0xCCEE CC-Component ID, EE-Error code

So according to the ph_Status.h, it's an error from RC communication in BAL Component Code.

Is someone have a hint or a solution to that particular issue ? 

Thanks a lot in advance, 

Florian Jouffreau

0 项奖励
回复
1 回复

1,466 次查看
catalin_alb
Contributor I

Good day,

I have the CLRC66303 connected over i2c to the Raspberry pi. I see the address "2b" with i2c detect.

Is there any example in C or Python just to see if the whole thing it is working ? 

Thank you,
Catalin 

0 项奖励
回复