Use the internal flash in rt1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use the internal flash in rt1064

2,977件の閲覧回数
jalvarez96
Contributor I
 
Hi,
I am trying to use the internal flash of the RT1064 based on this example (https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-the-RT1064-on-chip-flash-as-NVM/ta-p/...) and I am getting this error.
 
Hard Fault (HFSR)
FORCED (30) Indicates a forced hard fault, generated by escalation of a fault with configurable priority that cannot be handled, either because of priority or because it is disabled.
 
Usage Fault(UFSR)
UNDEFINSTR (0) Undefined instruction.
 
Thanks
0 件の賞賛
返信
5 返答(返信)

2,955件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Could you please tell me what SDK version are you using and if you are using an RT1064-EVK?

 

Regards,

Daniel.

0 件の賞賛
返信

2,950件の閲覧回数
jalvarez96
Contributor I

Hi,

SDK version: 2.14.0.

Board: MIMXRT1064 - EVK

Regards,

Julian

0 件の賞賛
返信

2,935件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @jalvarez96,

 

I followed the steps mentioned in the article and seems to be working on my side.

Could you please double check? Or please share with me the exact changes you made in your project.

DanielRuvalcaba_0-1706818742983.pngDanielRuvalcaba_0-1706818742983.png

 

Regards,

Daniel.

 

 

0 件の賞賛
返信

2,890件の閲覧回数
jalvarez96
Contributor I

Hi Daniel

In my project I included the functions related to the management of FLASH memory within a library (C Static Library). The functions declared in the library are the same as those in the "flexspi_nor_polling_transfer" example. The application with the functions declared outside the library (within the same project) works correctly but with the functions declared in the library does not.

Another fact, the project also works correctly with the link of the application to RAM (ignore the flash). With the latter configuration, the functions for managing the FLASH memory are included in the static library.

Regards,

タグ(1)
0 件の賞賛
返信

2,859件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Are you trying flexspi_nor_polling_transfer example or your own application?

I would recommend you to first try to replicate the article. Once you are able to use the internal flash, try to replicate the process in your application.

Regards,

Daniel.

0 件の賞賛
返信