Updates for erratas?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updates for erratas?

1,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AchimKraus on Tue Apr 08 08:29:26 MST 2014
I found two workarounds for errors in USB-ROM of the 1347 in the LPCOPEN sources
(cdc_main.c,
"WORKAROUND for artf32289 ROM driver BUG:" and
"WORKAROUND for artf44835 ROM driver BUG:").
Is there any frequently updated list of known bugs/errors/workarounds?
The erratas seems to be updated too rarley.
Though the errors have numbers, I guess there is a bug tracking system.
Is this accessable from the web?
ラベル(1)
0 件の賞賛
返信
1 返信

1,508件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Fri May 09 17:40:52 MST 2014
We always place known bugs/errors with workarounds if they exist in the errata sheet. The two workarounds you are mentioning here have not gotten placed into the errata sheet yet but they will be soon.

We do have an internal bug tracking system that we use here but we do not open this up to the public.

Thank you for pointing out these missing errors, we always appreciate these notices and we will work quickly to resolve them.

0 件の賞賛
返信