Unused USB pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unused USB pins

1,911件の閲覧回数
jpowning
Contributor I

Regarding the USBn_3V3 pins, the datasheet says "Tie to VBAT_DCDC or connect to ground . If not using USB and using 1.8 V supply, USBn_3V3 can be connected to 1.8 V." This is confusing. If you are not using USBn, and it says it can be connected to ground, then why not connect it to ground (to minimize supply current)?

0 件の賞賛
返信
3 返答(返信)

1,901件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi jpowning 

What's the part number?

Thanks,

Jun Zhang

0 件の賞賛
返信

1,893件の閲覧回数
jpowning
Contributor I

Hi - the part I am using is LPC55S16JBD100. Thanks for your interest.

0 件の賞賛
返信

1,876件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Please use the DS recommended design for unused USB pins. This is related with on chip HW design.

you should consider USB low power mode or disable USB domain to lower the power consumption.

Thanks,

Jun Zhang

0 件の賞賛
返信