Unresponsive to Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unresponsive to Programming

1,344件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ksoneda on Tue Jan 12 09:14:33 MST 2016
Failed on connect: Ee(07). Bad ACK returned from status - wire error.
Connected. Was: NotConnected. CpuID: 00000000. Info: WIN64HS12

I was running debug mode on my LPCXpresso LPC11C24 Board when I started getting the above error message.

I tried debugging using an LPC-Link2 it didn't even appear on the list of debug options.

Also, the LED1 on the LPC-Link side of the board no longer lights up.

Anyone have any ideas what might be going on?
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,328件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ksoneda on Tue Jan 12 11:44:21 MST 2016
It works great now

Thank you R2D2
0 件の賞賛
返信

1,328件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Jan 12 09:27:04 MST 2016
Switch to ISP:

https://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

as shown here:

https://www.youtube.com/watch?v=chFv1EiZcYo
0 件の賞賛
返信

1,328件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ksoneda on Tue Jan 12 09:19:01 MST 2016
Full debug log

LPCXpresso Debug Driver v8.0 (Nov 17 2015 10:46:16 - crt_emu_lpc11_13_nxp build 305)
Failed on connect: Ee(07). Bad ACK returned from status - wire error.
Connected. Was: NotConnected. CpuID: 00000000. Info: WIN64HS12
Error 0: OK
Last sticky error: 0x0 AIndex: 0
No debug bus (MemAp) selected
DAP Speed test unexecuted or failed
Debug protocol: SWD Frequency 50 KHz. RTCK: Disabled. Vector catch: Disabled.
(100) Target Connection Failed
0 件の賞賛
返信