Unconnected Pin of LPC1759FBD80 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unconnected Pin of LPC1759FBD80 ?

2,028 Views
abhilashsonawan
Contributor I

Hello,   

    Using LPC1759FBD80 in my design attach sheet shows the details of Unconnected (NC) pin of MCU.

   Please provide solution regarding proper termination as EMI/EMC point of view for NC pins. Weather it requires pull up /pull down/floating?

Labels (1)
0 Kudos
Reply
1 Reply

1,917 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

For the NC pins of the EMC/EMI you can leave these pin floating or connected to ground, with either these two options you shouldn't have any problem.

Hope it helps! 

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply