Unable to program LPC1347 using JTAG pins.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to program LPC1347 using JTAG pins.

3,497 Views
shreelaxminair
Contributor I

Hi all,

I am using LPC1347. In this controller TMS and SWDIO are not multiplexed.

So I have used Ulink Pro to program the controller via JTAG. However the device does not get detected via JTAG. Programming via SW is possible though. Can any one help and explain why programming via JTAG is not happening?

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

3,290 Views
thefallguy
Contributor IV
0 Kudos
Reply

3,287 Views
shreelaxminair
Contributor I

Ok

0 Kudos
Reply

3,287 Views
rolfmeeser
NXP Employee
NXP Employee

The JTAG port provides access to boundary scan only.

CPU debugging and flash programming can be done solely through the SWD port.

This is not an SWJ-DP.

0 Kudos
Reply

3,287 Views
shreelaxminair
Contributor I

Thanks for the reply.

By the way how does debugging & boundary scan differ from each other?

0 Kudos
Reply