Unable to program LPC1347 using JTAG pins.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to program LPC1347 using JTAG pins.

3,538 次查看
shreelaxminair
Contributor I

Hi all,

I am using LPC1347. In this controller TMS and SWDIO are not multiplexed.

So I have used Ulink Pro to program the controller via JTAG. However the device does not get detected via JTAG. Programming via SW is possible though. Can any one help and explain why programming via JTAG is not happening?

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

3,331 次查看
thefallguy
Contributor IV
0 项奖励
回复

3,328 次查看
shreelaxminair
Contributor I

Ok

0 项奖励
回复

3,328 次查看
rolfmeeser
NXP Employee
NXP Employee

The JTAG port provides access to boundary scan only.

CPU debugging and flash programming can be done solely through the SWD port.

This is not an SWJ-DP.

0 项奖励
回复

3,328 次查看
shreelaxminair
Contributor I

Thanks for the reply.

By the way how does debugging & boundary scan differ from each other?

0 项奖励
回复