Uart

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Uart

1,527 次查看
Anshu
Contributor I

Hi

I was trying to communicate the compass with lpc54s10 microcontroller evk board using uart.

I used j13 connector pin 13 for tx and pin 15 for rx of evaluation board.

I was not receiving data when i connected rx to pin 15 and tx to pin 13. Data started coming once i reversed the connection.

Why data is coming in reverse condition. Is there any pblm with uc pin or uc respective pin got damaged or not.

 

0 项奖励
回复
1 回复

1,347 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the LPC540xx board, as you have seen that the pin13 of J13 is the TX pin of Uart of LPC540xx, it must be connected to the RX pin of your compass.   The pin15 of J13 is the RX pin of Uart of LPC540xx, it must be connected to the TX pin of your compass.

Pls have a check.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1681697460241.pngxiangjun_rong_0-1681697460241.png

 

0 项奖励
回复