USBHS example project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBHS example project

2,332件の閲覧回数
enricobe
Contributor II

Hi all,

are there any SDK examples for USB1 HS HOST controller?

Several OHCI projects are already provided for USB0 port.

Regards,

Enrico

ラベル(2)
タグ(2)
1 返信

2,061件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

There is a demo code that you can use as reference like:

usb_keyboard2mouse(this is a dual usb demo)

boards\lpcxpresso54608\usb_examples\usb_keyboard2mouse

 

In addition attached to this thread you can find 2 examples, the lpc5460x_mgn_0323.7z is a reference project for USB1 as device, this use the the ROM API.

 

hots_usb.zip is the hands on projects for USB step by step.

 

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信