USB voltage supply for full/high-speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB voltage supply for full/high-speed

1,279 次查看
mikkelbjerring
Contributor I

I have been going over the documentation for the LPC546xx and have a question about the Vdd needed for USB 

this is on page 87 in the datasheet 

pastedImage_1.png

It is mention that you need a higher voltage to use USB full-speed than the USB high-speed 

any input to why this is the case ?

Br

Mikkel

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,179 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mikkel,

This is my opinion, I think the full-speed USB of LPC546xx uses the old usb IP as the other old LPC family, because of historical reason, the old USB IP requires that VDD voltage must be in the range from 3.0V to 3.6V.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复