USB voltage supply for full/high-speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB voltage supply for full/high-speed

1,259件の閲覧回数
mikkelbjerring
Contributor I

I have been going over the documentation for the LPC546xx and have a question about the Vdd needed for USB 

this is on page 87 in the datasheet 

pastedImage_1.png

It is mention that you need a higher voltage to use USB full-speed than the USB high-speed 

any input to why this is the case ?

Br

Mikkel

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,159件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mikkel,

This is my opinion, I think the full-speed USB of LPC546xx uses the old usb IP as the other old LPC family, because of historical reason, the old USB IP requires that VDD voltage must be in the range from 3.0V to 3.6V.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信