USB voltage supply for full/high-speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB voltage supply for full/high-speed

1,265 Views
mikkelbjerring
Contributor I

I have been going over the documentation for the LPC546xx and have a question about the Vdd needed for USB 

this is on page 87 in the datasheet 

pastedImage_1.png

It is mention that you need a higher voltage to use USB full-speed than the USB high-speed 

any input to why this is the case ?

Br

Mikkel

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,165 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mikkel,

This is my opinion, I think the full-speed USB of LPC546xx uses the old usb IP as the other old LPC family, because of historical reason, the old USB IP requires that VDD voltage must be in the range from 3.0V to 3.6V.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply