USB succeeding data transmission interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB succeeding data transmission interface?

2,279件の閲覧回数
BertrandR
Contributor II

Hello,

Newby with LPC, I am trying to setup VCOM communication on my custom board with a LCP55S16

I am using "peripherals tool" to try to set up with preset but I have a field in error and I don't understand at all what should be the value. I try from 0 to 255 without any result. Error should be some where else.

BertrandR_0-1673089502751.pngBertrandR_0-1673089502751.png

Thank you for your help

Bertrand

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

2,175件の閲覧回数
felix1
Contributor IV

Hi,

You need to setup two interfaces, CIC VCOM and DIC VCOM. These two interfaces map to three endpoints (Interrupt In, Bulk In and Bulk Out).

0 件の賞賛
返信

2,267件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think you can download SDK package from the link

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-s...

 

There is usb_device_cdc_vcom example, you can refer to the example

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1673231986826.pngxiangjun_rong_0-1673231986826.png

 

 

 

0 件の賞賛
返信