USB power needed even if USB is not used?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB power needed even if USB is not used?

1,303 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kraku on Tue Jan 05 14:29:27 MST 2016
A quick question:

Is USB power mandatory for the LPC43xx to work properly? If I don't use the USB, should it still be fed with VDD, etc.?

Thanks!
Labels (1)
0 Kudos
Reply
2 Replies

1,291 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kraku on Wed Jan 06 03:19:49 MST 2016
OK, thank you!
0 Kudos
Reply

1,291 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Wed Jan 06 01:45:52 MST 2016

Quote: kraku


Is USB power mandatory for the LPC43xx to work properly?



No!
0 Kudos
Reply