USB power needed even if USB is not used?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB power needed even if USB is not used?

1,271件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kraku on Tue Jan 05 14:29:27 MST 2016
A quick question:

Is USB power mandatory for the LPC43xx to work properly? If I don't use the USB, should it still be fed with VDD, etc.?

Thanks!
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,259件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kraku on Wed Jan 06 03:19:49 MST 2016
OK, thank you!
0 件の賞賛
返信

1,259件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Wed Jan 06 01:45:52 MST 2016

Quote: kraku


Is USB power mandatory for the LPC43xx to work properly?



No!
0 件の賞賛
返信