USB device was not supported by SDK, and USB device/stack missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB device was not supported by SDK, and USB device/stack missing

975 Views
waliwalabo
Contributor I

Hi,

 

I download the lastest the SDK for board LPC55S69 and tried the USB VCOM example. It works.

 

Then I try to add USB VCOM in my project by config tool-peripherals and no component was supported by the sdk. I change to all component and randomly used one and the tool complained that USB device/stack is missing.

waliwalabo_0-1750186238178.png

 

Did I download the wrong SDK? I got it from the SDK builder and selected all components available. Or is it ture that this board's SDK don't support any USB peripherals? The only way to use USB vcom is copy the example code?

 

0 Kudos
Reply
1 Reply

942 Views
Habib_MS
NXP Employee
NXP Employee

Hello @waliwalabo,
Please select the option "All" instead of "Supported by the SDK package", as the USB driver was added in previous SDK versions. Also, I highly recommend use the latest version available, as shown the next image:

Habib_MS_0-1750286633073.png


BR
Habib

0 Kudos
Reply