USB device was not supported by SDK, and USB device/stack missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB device was not supported by SDK, and USB device/stack missing

986件の閲覧回数
waliwalabo
Contributor I

Hi,

 

I download the lastest the SDK for board LPC55S69 and tried the USB VCOM example. It works.

 

Then I try to add USB VCOM in my project by config tool-peripherals and no component was supported by the sdk. I change to all component and randomly used one and the tool complained that USB device/stack is missing.

waliwalabo_0-1750186238178.png

 

Did I download the wrong SDK? I got it from the SDK builder and selected all components available. Or is it ture that this board's SDK don't support any USB peripherals? The only way to use USB vcom is copy the example code?

 

0 件の賞賛
返信
1 返信

953件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @waliwalabo,
Please select the option "All" instead of "Supported by the SDK package", as the USB driver was added in previous SDK versions. Also, I highly recommend use the latest version available, as shown the next image:

Habib_MS_0-1750286633073.png


BR
Habib

0 件の賞賛
返信