USB PID encoding error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB PID encoding error

1,364 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jonas2 on Tue Sep 03 05:50:51 MST 2013
I try to set up the USB module in device slave mode and connect it to a Win XP pc. The first interrupt i get is DEV_STAT and the second is ERR_INT. When i get the ERR_INT I run the Get Error Code command and get error code 0x1, PID Encoding Error. What might the reason be for this error? Win XP shows the message "USB Device Not Recognized". I use a LPC1778.

标签 (1)
0 项奖励
回复
1 回复

1,338 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jonas2 on Wed Sep 04 00:17:35 MST 2013
I found the problem. The usb clock frequency was 60 MHz. I set it to 48 MHz and now I don't get the error.
0 项奖励
回复