USB PID encoding error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB PID encoding error

1,373 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jonas2 on Tue Sep 03 05:50:51 MST 2013
I try to set up the USB module in device slave mode and connect it to a Win XP pc. The first interrupt i get is DEV_STAT and the second is ERR_INT. When i get the ERR_INT I run the Get Error Code command and get error code 0x1, PID Encoding Error. What might the reason be for this error? Win XP shows the message "USB Device Not Recognized". I use a LPC1778.

Labels (1)
0 Kudos
Reply
1 Reply

1,347 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jonas2 on Wed Sep 04 00:17:35 MST 2013
I found the problem. The usb clock frequency was 60 MHz. I set it to 48 MHz and now I don't get the error.
0 Kudos
Reply