USB Mass Storage LPC1768 SDCard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Mass Storage LPC1768 SDCard

1,624 Views
contr2889
Contributor III

Hi everyone,

    I am working with LPC1768 and now i need to use this device as USB Mass Storage, connect it to a computer and see files stored in a SD card with SPI interface. I am new using the USB Interface for this type of application, then first of all, is it possible to do that? what i must read or there are some examples to check? I am attentive to your comments.

Best Regards.

0 Kudos
Reply
1 Reply

1,610 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

For the USB mass storage device example you can take a look to the Keil MDK software package for the MCB1700 Board which includes an example of this.

image.png

 Also, I recommend you to check AN11070 that describes how to use the SPI/SSP interface on the LPC1700 family MCU to access Secure Digital Card (SDC) or Multi Media Card (MMC).

Hope it helps!

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 Kudos
Reply