USB Mass Storage Device + AT45DB161

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Mass Storage Device + AT45DB161

2,105件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nesarian on Fri Apr 27 05:13:47 MST 2012
Hi dear friends
Please Help me to write a program to read and write through USB Mass Storage Device
DataFlash = AT45DB161
NXPUSBLib = Example MassStorageDevice
Thanks
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Wed Jun 20 10:22:48 MST 2012
We added SPIFI support to the mass storage device example only for the NGX Xplorer boards. You will find this code at the bottom of the BSP file for this board: \libraries\BSP\NGX\bsp_NGX.c

We did not include this support for the Hitex A4 board because the memory device used has a 256k sector size and there was not enough internal SRAM to handle the required cache.

The code that does the actual interfacing to the SPIFI device is in a library that is linked in to this example. We do not provide source code in this library.
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nesarian on Fri Jun 15 23:11:41 MST 2012
Hi
Thanks for new version
But Quad SPIFI storage medium to the Mass Storage Class device was Not Found
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Tue May 29 17:53:25 MST 2012
We will be releasing v0.95 of nxpUSBlib in a week or two which includes a MSC example that accesses SPIFI flash. Unfortunately it will not be referencing this exact part.
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nesarian on Sat May 26 02:10:37 MST 2012
Hi dear friends
Why you dont give me Answer?!! :-{ :-(
Thanks
0 件の賞賛
返信