USB Mass Storage Class Device Example on LPCOpen 2.05

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB Mass Storage Class Device Example on LPCOpen 2.05

跳至解决方案
9,464 次查看
vrakeshm13
Contributor I

Hi,

Is there any USB Mass Storage Class Device example available for LPC1347 on LPCOpen v2.05? Kindly please share if it is available. 

Thanks & Regards,

Rakesh

标签 (3)
0 项奖励
回复
1 解答
9,396 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @vrakeshm13 

Yes, you can refer to it.The APIs almost the same, they are USB ROM API.

UM meaning UM10524. The APIs are included in LPCopen.

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
3 回复数
9,446 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @vrakeshm13 

Sorry there is no MSC example for lpc1437, there is usbd MSC API in UM-> 11.5.35 USBD_MSC_API and 11.5.36.

 

BR

Alice

0 项奖励
回复
9,441 次查看
vrakeshm13
Contributor I

Hi @Alice_Yang,

Thanks for the reply. Could you please share UM document? Also, I found below link which has MSC example for LPC11xx, so can I use this example as reference for development I hope same API's are available for LPC1347. 

https://community.nxp.com/t5/LPC-Microcontrollers/LPCopen-2-x-and-USB-Mass-Storage/m-p/523836?profil...

Thanks,

Vijay Rakesh.

0 项奖励
回复
9,397 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @vrakeshm13 

Yes, you can refer to it.The APIs almost the same, they are USB ROM API.

UM meaning UM10524. The APIs are included in LPCopen.

 

BR

Alice

0 项奖励
回复