USB Drivers for CDC CLASS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Drivers for CDC CLASS

2,627件の閲覧回数
TEMCEFF
Contributor IV

For the CDC class, Is there any USB Drivers are available for the LPC4357 Controller? 

ラベル(5)
0 件の賞賛
返信
1 返信

2,539件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Avinash, I hope you're doing well!

 

USB examples implementing the CDC Class and others are included with the LPC-Open package for the LPC43xx line of MCUs, which can be downloaded from the following page of our website:

LPCOpen Software for LPC43XX | NXP  

 

These LPC-Open Packages are also included with the MCUXpresso IDE Installation, and can be imported into MCUXpresso by clicking on the "Import projects from filesystem…" option in the Quickstart Panel, and choosing the corresponding LPC-Open Package for your board.

 

There's examples for the CDC Class with UART and VCOM.

 

Please let me know if you need any more information.

 

Take care, best regards,

Sebastian

0 件の賞賛
返信